LPC 3250 I2C transmission issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 3250 I2C transmission issue

810件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vikhyathk on Mon Oct 19 22:10:51 MST 2015
I am facing a problem with i2C transmission using LPC3250. I m using processor to interface FPGA with device id 0xA0. So the first data I put into '0x400a8000' (I2C2_TX) register is '0x1A0' and I see in the oscilloscope that start condition is generated and acknowledgement is present.

But Whenever I send a data byte later  with LSB bit '1', the same data is being resent with LSB bit made '0'.
Example: If I put "11011001' into the register '0x400a8000' (I2C2_TX) Data found in scope is ["11011001" 'Ack bit' "11011000"'Ack bit']..
'Ack bit' is '0'.

Can anybody help me to solve the issue.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)