LPC 3240 : MAC Receive stops after some time when multicast is enabled.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 3240 : MAC Receive stops after some time when multicast is enabled.

859 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aneejosep on Wed Nov 25 19:28:57 MST 2015
I am facing an issue that LPC3240 MAC Receive stops after some time when multicast is enabled. When multicast enable bit is set, some long packets and mac internal errors are reported. And after some time Rx Done interrupt is never triggered. I am using LwIP integrated with the board. Any reasons for this behavior?? Could someone please help? Thanks.
AJ.
Labels (1)
0 Kudos
Reply
0 Replies