LPC 17XX SERIAL DRIVERS IN LINUX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 17XX SERIAL DRIVERS IN LINUX

1,425 Views
deepakachar
Contributor I

Hello,

My name is Deepak. I am from India. I am using LPC 17xx Serial drivers for Windows for application in CAN To USB converter. I need to port my application to Linux. I have doubt that does Linux requires any LPC drivers for serial communication. At present I have read the Vendor ID and Product ID using Libudev Libraries. I am trying to write the data of 9 bytes. I am not getting any response from the host firmware. Where as I am getting response in Windows using my API's. Presently I am developing API's for Linux. I mentioned Vendor ID and Product ID here. Please me regarding this.

Vendor ID: 1fc9

Product ID: 2002

Regards

Deepak, India

0 Kudos
Reply
1 Reply

1,325 Views
soledad
NXP Employee
NXP Employee

Hello,

 

You can download the driver from the next link:

http://www.ftdichip.com/Drivers/VCP.htm

 

I hope this helps!!

Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply