LPC 1768 Code for USB host Mass Storage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 1768 Code for USB host Mass Storage

1,256 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ankit_Y on Sat Jun 04 04:35:47 MST 2016
I am working on LPC1768, and want to code it for USB host mass storage which can able to create file, write file, read file, delete the file and format the USB device. There is a code of USB Host mass storage in Kiel but i can't able to port it to LPC Xpresso.

Please help me in this. or provide any library or code for the above.

Thank you in Advance.
Labels (1)
0 Kudos
Reply
1 Reply

1,058 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply