LPC驱动1024*768屏幕显示水波纹

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC驱动1024*768屏幕显示水波纹

997 Views
saidadiao
Contributor I

使用LPC1788的MPU,驱动1024*768的24位TFT屏幕,LCD时钟为19.2M的时候,屏幕显示图像正常,但有水波纹,频闪现象,LCD时钟为32M的时候,屏幕频闪现象消失,但是出现花屏现象,屏幕撕裂

Labels (1)
0 Kudos
Reply
7 Replies

972 Views
Alice_Yang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

969 Views
saidadiao
Contributor I
我想知道,LPC1788支持的1024*768分辨率,32位屏的最大LCD时钟频率是多少
0 Kudos
Reply

942 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @saidadiao 

Are your sure 32 bits? Or 24 bits? 

And do you want to know the max clock source of LPC1788 LCD clock frequency or your LCD frame? 

You can send the datasheet of LCD to me.

 

BR

Alice

0 Kudos
Reply

936 Views
saidadiao
Contributor I
刚回复了屏的规格书,屏颜色深度是24bit的
0 Kudos
Reply

859 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @saidadiao 

1) From the DS of LCD you send, the frequency is out of the LPC1788 support:

Alice_Yang_0-1703582184044.png

 

 

2) Please check the configuration of your LCD driver:

HSW HFP HBP VSW VFP VBP

 

BR

Alice

 

 

0 Kudos
Reply

838 Views
saidadiao
Contributor I

谢谢,问题已经解决了

0 Kudos
Reply

937 Views
saidadiao
Contributor I
 
0 Kudos
Reply