LPC驱动1024*768屏幕显示水波纹

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC驱动1024*768屏幕显示水波纹

868件の閲覧回数
saidadiao
Contributor I

使用LPC1788的MPU,驱动1024*768的24位TFT屏幕,LCD时钟为19.2M的时候,屏幕显示图像正常,但有水波纹,频闪现象,LCD时钟为32M的时候,屏幕频闪现象消失,但是出现花屏现象,屏幕撕裂

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

843件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

840件の閲覧回数
saidadiao
Contributor I
我想知道,LPC1788支持的1024*768分辨率,32位屏的最大LCD时钟频率是多少
0 件の賞賛
返信

813件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @saidadiao 

Are your sure 32 bits? Or 24 bits? 

And do you want to know the max clock source of LPC1788 LCD clock frequency or your LCD frame? 

You can send the datasheet of LCD to me.

 

BR

Alice

0 件の賞賛
返信

807件の閲覧回数
saidadiao
Contributor I
刚回复了屏的规格书,屏颜色深度是24bit的
0 件の賞賛
返信

730件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @saidadiao 

1) From the DS of LCD you send, the frequency is out of the LPC1788 support:

Alice_Yang_0-1703582184044.png

 

 

2) Please check the configuration of your LCD driver:

HSW HFP HBP VSW VFP VBP

 

BR

Alice

 

 

0 件の賞賛
返信

709件の閲覧回数
saidadiao
Contributor I

谢谢,问题已经解决了

0 件の賞賛
返信

808件の閲覧回数
saidadiao
Contributor I
 
0 件の賞賛
返信