LCP55S69 enter isp mode after power on

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCP55S69 enter isp mode after power on

1,360件の閲覧回数
wpro
Contributor I

  LCP55S69 enter isp mode after power on, but I didn't do anything to make the chip go into isp mode. the board is shown in Figure 1.

  Use FlashMagic check flash region 0 is all blank as Figure 2.

  At the same time, the swd also failed to connect.
  What can I do to get the swd back to normal.
 
20230707-171242.jpg

 

 

Figure 1

wpro_1-1688720962867.png

Figure 2

wpro_2-1688721116689.png

 

 

0 件の賞賛
返信
1 返信

1,335件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @wpro 

I hope you are doing well.

When there is no valid image present in the flash memory, or in this case no image available, the MCU will enter into ISP mode automatically.

Regarding  the swd also failed to connect  entering into ISP mode should not represent an issue to debug via SWD. In some casuses it ISP mode could help to regain debug access.

Would you detail how are you attempting to program by SWD and any error message related? Also, if  you made any setup into MCU's protected flash region (PFR). The PFR could be used to lock SWD access.

All the best, 

Diego

タグ(1)
0 件の賞賛
返信