LCP54S018M DMA driver questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCP54S018M DMA driver questions

2,616件の閲覧回数
carson_cummins
Contributor I

Hello all,

I'm a developer implementing DMA to transfer transmit only data (no recieve) to multiple flexcomm ports. I have a few questions:

 

1. I'm using the latest 2.8.0 SDK with DMA driver files included (fsl_dma & fsl_spi_dma .c/.h). There is no definition for FSL_FEATURE_DMA_DESCRIPTOR_ALIGN_SIZE. Can someone point me in the right direction as to what this should be?

2. There is no definition that matches the description of the DMA_ALLOCATE_LINK_DESCRIPTOR(nextDesc) macro as discussed on line 866 -881 in fsl_dma.c. I see a definition of DMA_ALLOCATE_LINK_DESCRIPTORS (with an 'S') but it appears to function differently than described in the comment.

3. I'm encountering an issue with linked list DMA to SPI peripheral transfers. On every flexcomm channel I've set up, there is an intermittent extra bit inserted in to the data stream that is shifting the data going out by one. I'm interfacing with WS2812B LEDs and this is causing them to flicker. The data being transferred has been verified as correct so I'm not sure where this extra bit is coming from.

Thank you in advance.

0 件の賞賛
返信
4 返答(返信)

2,584件の閲覧回数
carson_cummins
Contributor I

**

0 件の賞賛
返信

2,598件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello carson_summins,

I recommend you open the SDK demo  "dma_linked_transfer", you can find the

description of your two question.

1. " FSL_FEATURE_DMA_DESCRIPTOR_ALIGN_SIZE"

Alice_Yang_1-1600329067643.pngAlice_Yang_1-1600329067643.png

2.  "DMA_ALLOCATE_LINK_DESCRIPTOR" is one of DMA descriptor of "DMA_ALLOCATE_LINK_DESCRIPTORS".

Alice_Yang_2-1600329168631.pngAlice_Yang_2-1600329168631.png

 

 

 

 

 

0 件の賞賛
返信

2,580件の閲覧回数
carson_cummins
Contributor I

Wonderful, thank you. Is there anything you can infer from #3? I've looked at the code examples provided by NXP and they don't really cover an instance where DMA is being used without needing RX. I've got the setup somewhat functional sending data only DMA->SPI but I don't think the provided driver file was designed with ignoring RX data in mind. Do you or anyone else know of any example code that I could view?

0 件の賞賛
返信

2,573件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello carson_cummins,

Recommend you using  logic analyzer check transfer signal. 

0 件の賞賛
返信