LCP176x pin mux tool, pin table formating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCP176x pin mux tool, pin table formating

1,386件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GRandy on Fri Aug 09 12:51:07 MST 2013
Two questions:

I see there is a pin mux tool for the LPC177x, but is there a pin mux tool for the LPC176x?

Is there a table, xls, csv, etc file available of the LPC176x different than from the datasheet?  The NXP datasheets do not format the pin tables in a way conducive to copying-and-pasting the information into a spreadsheet for easy manipulation.  When I use a spread sheet to keep track of my pin assignments, and then import that spreadsheet into my PCB design tools to define the schematic symbol, I first have to manually type (or copy and paste) the different options for each pin.  Which is a touch tedious.  Are there any better options available to me?

-Randy
ラベル(1)
0 件の賞賛
返信
1 返信

1,238件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Wed Aug 14 14:15:00 MST 2013
Randy
There is no pin mux tool available for the LPC176x family.  Attached is a text file with the pin functions for the LPC1768.  This can easily be imported into a spreadsheet using space delimiting.  Hopefully this is useful for you.
0 件の賞賛
返信