LCD controller outputting something different than framebuffer content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD controller outputting something different than framebuffer content

1,119 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by egnascimento on Thu Nov 26 04:49:17 MST 2015
Hi,
I'm using LPC1857 with a R61509 LCD and SDRAM with CS0.

I do test SDRAM before anything so it seems to be working fine. I'm working with RGB 16bit mode 565.

I fill SDRAM with 0x1F which should be pure blue then configure framebuffer to point to 0x1C000000.

The problem I see is that after everything is set, display is only noise with several colors. I checked with scope and I do see some pulses on Red and Green lines which is not expected since framebuffer has only blue info.

Can anyone see what I'm missing?

Thanks!
Labels (1)
0 Kudos
Reply
1 Reply

1,108 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by egnascimento on Fri Nov 27 06:19:22 MST 2015
Anyone? Would the LCD picture help someway?
0 Kudos
Reply