Jtag debugging issue with my custom build circuit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Jtag debugging issue with my custom build circuit

3,473 次查看
rajeshjat56
Contributor I

I am not able to debug my lpc 2292 board, i think i am having some hardware issue, signals are as per schematic image.

I have attached my JTAG connector and controller connection.

Rtclk is pull down with 4.7k resistor and boot loader is also pull down for programing.

Please help me,it is not debugging but programing from JTAG.

标签 (3)
标记 (3)
0 项奖励
回复
3 回复数

3,305 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

See Design considerations for debug

Thanks and regards,

MCUXpresso Support 

0 项奖励
回复

3,305 次查看
rajeshjat56
Contributor I

I have done circuit as debug circuit design consideration mention in above link, but still i am not able to debug and after debugging option selection, it goes into directly to exception vectors, infinite loop and code run,but not single step debug.

0 项奖励
回复

3,305 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Rajesh,

As you said " it goes into directly to exception vectors, infinite loop and code run,but not single step debug.", it seems that you have downloaded the code to flash, the JTAG circuit is fine, but the code has issue so that it can not run. Pls try to check your code.

BR'

Xiangjun Rong

0 项奖励
回复