JPEG file over USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JPEG file over USB

1,358 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ahmed13 on Thu Jul 03 01:03:08 MST 2014
Hello everyone,

I'm using a LPC43xx, and I want to send pictures from the SD card to the PC over USB.

I'm able to read and send data from the SD card to the PC (using f_open and f_read like in the example LPCopen sdmmc and using the WriteEP function to send the data over bulk IN USB)

On host side I have an app that is using external JPG library and re-assembling the data to make it a jpg file.
(For the moment I'm sending a PNG file from the SD card, sending only the data avoiding the headers).


The thing is I'm not able to re build a correct image, is there any function dealing with jpg for LPC ?
If anyone have already deal with this subject feel free to answer.

thank you very much,

Regards, Ahmed.


Labels (1)
0 Kudos
Reply
2 Replies

1,348 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Jul 03 16:24:45 MST 2014
hi,

Have you tried the USB Mass storage class example ?

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc43xx-packages

Thanks,

NXP Technical Support
0 Kudos
Reply

1,348 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Thu Jul 03 11:50:09 MST 2014
probably an endian issue
0 Kudos
Reply