Is the LPC4337JET256 compatible with the LPC1837JET256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the LPC4337JET256 compatible with the LPC1837JET256

1,120 Views
tonyvinto
Contributor I

Can I drop this Cortex M4 onto my board in place of the Cortex M3 part and expect it to work?  The datasheet makes em loop awfully compatible but it does not come out and say it is.  I want to make use of the extra clock speed and the math co-processor.  So I would only expect to modify initialization code for the 204MHz.

Are there any gotchas that I need to know about.  

What about eratta?  The 1837 had that CAN problem in rev "-".  Has the rev A of the 4337 been released with that fix?

Thanks

0 Kudos
Reply
1 Reply

1,030 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Tony Vinto,

Can I drop this Cortex M4 onto my board in place of the Cortex M3 part and expect it to work?

Yes, and LPC1800's pin assignment is compatible with the LPC4300.

The bug is also exist in the initial device revision of the LPC4337, but not in the second revision.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply