Interfacing LPC1768 with T6963 240x64 glcd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing LPC1768 with T6963 240x64 glcd

2,971件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by awadhesh on Sun Mar 01 23:59:14 MST 2015
Hi,
I have tried my best to interface T6963 with LPC1768, but  LCD does not show anything. However same thing working with 89v51RD2.

I am also getting status is ready with both controller, whereas first one is not working.

Please let me know if anyone have done it or any suggestion for it.

Thanks & Regards,
Awadhesh

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,764件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Thu Mar 05 08:21:06 MST 2015
DB0 - DB7 are bi-directional and will output 5V onto the LPC1768.  Let us hope you used some 5v tolerant pins.
you did not look very hard
http://198.101.240.182/content/forum/starting-glcd-240x128-lpc1768-microcontroller
and I found lots of google hits.
0 件の賞賛
返信

2,765件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by awadhesh on Tue Mar 03 21:27:52 MST 2015
Its written that data lines, CE, WR, RD CD having high logic from VDD-2.2V to VDD.
0 件の賞賛
返信

2,765件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mazyarseyedi on Mon Mar 02 09:33:16 MST 2015
How you translating logic
I mean LPC is 3.3V but controller is 5v
0 件の賞賛
返信