Integrate DLMS protocol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrate DLMS protocol

1,918 Views
smishra125
Contributor I

I am using LPC55S69-EVK Evaluation Board having LPC55S69JBD100 controller. I need to integrate DLMS protocol via UART with this board. Can you suggest me the example projects or links to implement in this controller.

Thanks.

0 Kudos
Reply
2 Replies

1,904 Views
smishra125
Contributor I

@xiangjun_rong Thanks for the trying.

0 Kudos
Reply

1,908 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked the DLMS (IEC 62056), I suppose there is not DLMS code or related document for mcu like LPC, Kinetis..., you have to implement it yourself.

sorry for not helping you

BR

XiangJun Rong

0 Kudos
Reply