Infrared configuring in lpc3250

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Infrared configuring in lpc3250

1,388件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akarshana on Wed Jan 01 21:52:51 MST 2014
hai

In my project I want use LPC3250-IR_RX pin,

Is there any configuration required in kernel? If it is can any one tell me how to configuring kernel,

and what is the data format while reading this pin?

Is there any example code for IRDA communication

thank you advance

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,332件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embeddedguy on Tue Mar 18 10:14:06 MST 2014
t
0 件の賞賛
返信

1,332件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Feb 06 16:32:46 MST 2014
Hi Akarshana,

Visit the following link for examples on IrDA in the UART  folder for LPC175x/6x.

http://www.lpcware.com/content/nxpfile/lpc175x6x-cmsis-compliant-standard-peripheral-firmware-driver...


Thanks

NXP Technical Support
0 件の賞賛
返信