Incorrect SPI flash connection in boot mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Incorrect SPI flash connection in boot mode.

1,098件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by a5856 on Tue Jul 24 08:18:55 MST 2012
Using oscilloscope, I found correct pin functions in SPI(SSP) boot mode:

P3.3 - SSP0_CK,
P3.6 - SSP0_SSEL,
P3.7 - SSP0_MISO,
P3.8 - SSP0_MOSI

Please check and correct Table 19 in Chapter 5.3 of user manual UM10503.

And what about "program mode" in DFUSec tool?
I don't find it in lpc_dfusec_v0.98aNS. There is only HDR/RAW mode...
ラベル(1)
0 件の賞賛
返信
1 返信

1,083件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Tue Jul 24 14:18:38 MST 2012
>And what about "program mode" in DFUSec tool?
>I don't find it in lpc_dfusec_v0.98aNS. There is only HDR/RAW mode...
This is available now in DFUSec v1.00.

http://www.lpcware.com/content/project/dfu-download-programming-utility-and-security-lpcdfusec-tool
0 件の賞賛
返信