Inconsistency between the system AHB clock control and UART configuration of LPC112x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inconsistency between the system AHB clock control and UART configuration of LPC112x

1,615 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tddian on Wed Jul 22 03:53:40 MST 2015
Hello all,

I am using the LPCXpresso1125 board, and there are some potential bugs/inconsistencies about the UART part and the system AHB clock control, both in the driver (lib_lpc_chip_112x) and the user manual (UM10839 for LPC112x, Rev. 1.0)

Firstly this board has three UART0/1/2, stated in page 4, line 1 in the user manual. Table 19 shows that the SYSAHBCLKCTRL supports up to bit 20, where bit 12, 19 and 20 are for enabling clock for UART0, 1 and 2 respectively. On the driver side, in chip.h line 98-100 the three UARTs are also accordingly defined.

On the other hand, in clock_112x.h file line 176-196 where the CHIP_SYSCON_CLOCK_T is defined, the bit 19 and 20 for SYSCON_CLOCK_UART1 and SYSCON_CLOCK_UART2 are missing, which is inconsistent against Table 19. Thereby with this driver library [u]the UART1 clock and UART2 clock are never reachable[/u].
More over, in uart_112x.c line 51-64, the function Chip_UART_Init() is supposed to initialize the given UARTx, but in line 53 it alsways enables the clock for UART0. That is, [u]the UART1 and UART2 will never be correctly initialized[/u] and can't be used at all.

This can be varified by replacing all the "LPC_UART0" to "LPC_UART1" in the example "periph_uart_rb".

Labels (1)
0 Kudos
Reply
2 Replies

1,598 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Sat Aug 15 05:01:01 MST 2015
The IOCON registers are all incorrect in iocon_112x.h. 

NOTE:  (CHIP_IOCON_PIO_T)  enum must be rewritten to match the documentation.  If you are using the NXP driver, you will be setting the wrong IOCON configuration for UART1 and UART2.

ie.

Change:
IOCON_PIO0_7 = (0x050 >> 2)

to:
IOCON_PIO0_7 = (0x0C8 >> 2),

0 Kudos
Reply

1,598 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Fri Aug 14 13:14:27 MST 2015
I noticed the same issues and corrected the driver to the documentation..., are you still having issues with UART1 and UART2?
0 Kudos
Reply