Implementing IEEE 1588 on an LPC43XX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing IEEE 1588 on an LPC43XX

1,966 Views
jonathansmith
Contributor III

I have a project using multiple LPC4333s, presently using a custom communications protocol to synchronise data samples and collect the sampled data across the devices. I am looking to change the communications protocol to something standard to help with future development and maintainability, and so am looking at connecting them all using the on board Ethernet and using the IEEE 1588 Precision Time Protocol to synchonise the devices.

Is there any example code to help me get started with this?  Any documentation other than the manual that is helpful?

Labels (3)
0 Kudos
Reply
1 Reply

1,853 Views
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, there is no related demo or doc using the IEEE 1588 Precision Time Protocol.

Regards 

Sol 

0 Kudos
Reply