ISP LPC54608

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISP LPC54608

1,544 Views
実奥山
Contributor II

Plese teach me how to progoramming(ISP) LPC54608(LPCXpresso54608 board) by Ethernet and UART.

Labels (1)
0 Kudos
Reply
1 Reply

1,368 Views
soledad
NXP Employee
NXP Employee

Hi,

You can check this in the user manual for the LPC54608, chapter 5.

https://www.nxp.com/docs/en/user-guide/UM10912.pdf 

Flash programming, and other related functions, are supported in several different ways:

• For details of USART In-System Programming, see Section 5.4.

• For details of I2C and SPI In-System Programming, see Section 5.5.

• For details of In-Application Programming, see Section 5.6.

• For details of USB programming, see Chapter 41 “LPC546xx USB ROM API”. The boot loader version can be read by ISP/IAP calls (see Section 5.4.5.13 or Section 5.6.6).


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply