IPC in LPC4300

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPC in LPC4300

2,221件の閲覧回数
katisr
Contributor I

Hello all,

I am new to LPC4300 and multicore. I saw few examples in LPCOpen. There were examples with RTOS and without.  As a beginner it is confusing if I should use RTOS or not.  I have attached the link where I found the examples LPCOpen Software for LPC43XX|NXP . My question is , is RTOS necessary for working in dual-core mode ? I just wanted to experiment the IPC with simple examples like  M4 turning ON LED and M0 turning it OFF.

0 件の賞賛
返信
1 返信

1,822件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

No, it is no necessary to work with a RTOS, however it is easier to manage both cores using the RTOS.

Please check the below document

https://community.nxp.com/docs/DOC-330811

 

In addition I suggest to check the application note AN11177 Inter Processor Communication,

AN11177: Inter Processor Communications.

 this appnote provides information about:

  • The API implementation for dual core communication on LPC43xx targets
  • How to include or exclude functionality by means of a platform-wise configuration file
  • System level settings and debug options to be aware of when changing the

configuration

Regards

Soledad