IAP on lpc11u3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IAP on lpc11u3

1,996 Views
sanketk
Contributor I

Hi,

I am using a lpc11y3x device. I want to implement In application programming for the same.

But I am not able to get,  how do I jump from the iap code to my main application.

Is there any application note for the same or some example code to refer.

Regards,

Sanket

0 Kudos
Reply
2 Replies

1,881 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sanket K,

    About the IAP usage, you can refer to our application note AN11511, there has the document and the code for your reference.

https://www.nxp.com/docs/en/application-note/AN11511.zip

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,881 Views
sanketk
Contributor I

The device is lpc11u3x

0 Kudos
Reply