IAP on lpc11u3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IAP on lpc11u3

1,993件の閲覧回数
sanketk
Contributor I

Hi,

I am using a lpc11y3x device. I want to implement In application programming for the same.

But I am not able to get,  how do I jump from the iap code to my main application.

Is there any application note for the same or some example code to refer.

Regards,

Sanket

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,878件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sanket K,

    About the IAP usage, you can refer to our application note AN11511, there has the document and the code for your reference.

https://www.nxp.com/docs/en/application-note/AN11511.zip

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,878件の閲覧回数
sanketk
Contributor I

The device is lpc11u3x

0 件の賞賛
返信