I2C driver in lpc4330

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C driver in lpc4330

1,052件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by siva4PM on Fri May 30 03:47:19 MST 2014
Hi guys,

Iam writing driver for I2C bus on platform lpc4330(Device EEPROM).

Iam not clear about the master of the bus, whether the microcontroller will be the master ?
if yes means which core will takes place M0 or M4!



Hope for your help. Thanks in advance!

Best regards,
PS
ラベル(1)
0 件の賞賛
返信
1 返信

1,023件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri May 30 11:30:52 MST 2014
Hi, Siva4PM,

the microcontroller should be the master. either core M0 or M4 can do the job.

good luck!
0 件の賞賛
返信