I am looking for a very low power LPC Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am looking for a very low power LPC Microcontroller

2,393 Views
doini
Contributor III

Hello,


I am used to work with the microcontrollers from the LPC family (Cortex M) and now I need a very low power LPC microcontroller to work on battery which need to last long, maybe half of year (of course I'll use some of its peripherals also, like timers, ADC,...). In the same time the microcontroller needs to have a big processing power, because during running at some intervals of time I need to manipulate a lot of data at once.
I was thinking of the LPC 54102 microcontroller for low power consumption and to use Cortex M4 with the main program and Cortex M0 only when needed, in order to save power.
 
Would you like to recommend the best LPC very low power microcontroller which could help me with processing also?
I would appreciate any answer.
 
Thank you,
Doini

0 Kudos
Reply
1 Reply

2,277 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Doinita Marcu,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, I'd like to know more information about your application, then I can give a better suggestion for you.
So I was wondering if you can answer these below inquiries.
1. Do you have particular requirements about the clock frequency,  size of flash and RAM, and peripherals?
2) What's the mean "manipulate a lot of data"?
Does it mean float calculation or data moving?
2) Will the MCU enter the low power after completing the data manipulation?

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply