How to use NXP's LPC546x and MFR4310 to realize FlexRay? need help.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use NXP's LPC546x and MFR4310 to realize FlexRay? need help.

881件の閲覧回数
geweilin
Contributor II

I'm using LPC546x and now want to add FlexRay interface to my board. So I think we can use EMC module with MFR4310 and TJA1080 as a solution.

But I have no idea how to achieve it. Expect someone can provide help from two aspects of hardware schematic diagram and software implementation method.

ラベル(2)
0 件の賞賛
返信
1 返信

815件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Weilin,

Regarding your question, first of all, I would like to remind you of the fact that the LPC546xx operating temperature range is from -40 °C to +105 °C, it does not meet the automotive quality standard, as far as I know that the Flexray is used in auto application. The MPC56xx/57xx, S32K are auto level processor.

Anyway, I think it is okay to use EMC module to access the MFR4310 as a SRAM with AMI(Asynchronous Memory Interface) mode, the LPC546xx provide the signals: address bus, data bus, control bus(/CS,/OE,/WR,BLS0/1).

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信