How to flash image on Custom board lpc54618?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash image on Custom board lpc54618?

1,761件の閲覧回数
subodhmankar
Contributor II

Hi,

I am able to use lpclink2 to debug my custom board.

But when I try to flash image using lpclink2, MCUXPRESSO IDE shows success but custom board doesn't get flashed.

What are the steps, tools and procedure I should follow to flash LPC54618 custom board?

Please provide me suggested links pr tools...

タグ(4)
0 件の賞賛
返信
1 返信

1,584件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Subodh Mankar,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
1. Firstly, you should use the correct demo for testing, you can build a SDK for LPC54618 via the following link:
2. Secondly, compare with the OM13092 to check the hardware circuit of LPC54618 custom board.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------