How to download SW on KL82 except with JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to download SW on KL82 except with JTAG

1,583 Views
andy_kim
Contributor IV

Hello,

We're planning to develop POS device using KL82.

According to UM11036,

There is a way of download software using JTAG.

And According to AN4835,

There are two ways of programming interfaces which are SWD/JTAG and EzPort.

However,

When I check the pinouts of KL82 datasheet, I can't found the EzPort on it.

 

I wonder if there is really other way to flash programming except with JTAG Interface.

 

Thanks,

Andy

0 Kudos
Reply
3 Replies

1,577 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi andy_kim,

   In fact, to KL82 chip, it contains the ROM bootloader, that means you can use the LPUART to download the code directly.

image.pngimage.png

   More details, I highly suggest you read the KL82 reference manual, the ROM bootloader chapter, and the KBOOT related document:

https://www.nxp.com/webapp/Download?colCode=KBTLDRUG

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuboot-mcu-...

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

0 Kudos
Reply

1,565 Views
andy_kim
Contributor IV

Dear Kerry,

Thanks for your prompt feedback.

As far as I know, KL81 and KL82 are pin to pin in HW perspective and are using Common bootloader.

Can we refer to KL82 documents including datasheet and reference manual instead of KL81.

 

We're looking forward to seeing your reply.

 

Thanks,

Andy

0 Kudos
Reply

1,563 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi andy_kim,

KL81 to add the Tamper Pins and DryICE features, if you don't use these secure module, you can refer to the KL82 reference manual.

KL81 reference needs to sign the NDA with the NXP side.

If you just want to use the ROM bootloader, you can use the KL82 reference manual.

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply