How to copy a project to a new project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to copy a project to a new project

58 Views
jDrum1
Contributor I

I have been developing a project in the MCUXpresso IDE (chip LPC11U68) for several years.

I would like to use the same chip on a different PCB and need to generate a new project in the workspace.

The problem seems to be

1)  I can copy a project and rename it and open it in the IDE.  However, the quickstart menu shows project:  CNew[none].   I assume that the settings folder and the .project file (both xml) both need to be implemented properly.   Additionally, the project tree in the workspace seems to be different in the copied version.

2) alternatively, I can use the new project wizard  and get the project CNewj .  Here, the project can be built but is otherwise empty.  In principle, I can copy the proper files into the new project and build again, but this will take a couple of hours.  (I need to repeat this process for two additional PCBs as well.)

Any suggestions?

jDrum1 (used to be jDrum) 

Labels (1)
0 Kudos
Reply
1 Reply

30 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @jDrum1 

Thank you for contacting us.

You can use the "Import Project" button in MCUXpresso IDE to import your project. I’ve recorded a short video demonstrating the detailed steps and attached it for your reference.

Please let me know if you have any questions.

 

BR

Alice

0 Kudos
Reply