How to configure timer as counter??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure timer as counter??

4,438 Views
rajani_sureja33
Contributor III

Please provide details on initialization of  timer as counter. I want to count fan rpm (pulses) on pin 1.0 (CTIN_3).

So basically i want to count the pulses on that pin for specific time interval.

Labels (1)
0 Kudos
Reply
6 Replies

4,208 Views
rajani_sureja33
Contributor III

Hi Sol, 

Please provide an initialization code for this.

Thanks,

Rajani

0 Kudos
Reply

4,208 Views
rajani_sureja33
Contributor III

Hi Sol,

I have go through this link but didn't find anything useful. Can you provide me how to do that in lpc1833 on 1.0 (CTIN_3).

Thanks,

Rajani

0 Kudos
Reply

4,208 Views
soledad
NXP Employee
NXP Employee

Please check the below thread and let me know if this helps.

Any example to use CAPTURE PINS as pulse counters? | www.LPCware.com 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,060 Views
k_sunilgupta
Contributor II

this link is not opening.

Tags (2)
0 Kudos
Reply

4,208 Views
soledad
NXP Employee
NXP Employee

Hello,

 

Could you please mention the device you are using?

Regards

Sol

0 Kudos
Reply

4,208 Views
rajani_sureja33
Contributor III

Hi Sol,

I am using LPC1833 device.

Thanks,

Rajani

0 Kudos
Reply