How running code from external SPI flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How running code from external SPI flash

3,563件の閲覧回数
germano
Contributor II

Hi! I have read that it is not recomended to run code from the SPI Flash memory, however the LPC546xx User manual says:

Code in the serial flash memory can be executed as if it was in the CPU’s internal memory space. This is accomplished by mapping the external flash memory directly into the CPU memory space

Where can i find examples of code execution for mi LPCXpresso54608?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

2,695件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Germán Ontivero,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
To provide the fastest possible support, I'd like to point you to a 
similar question which has been answered on our NXP community. 
Please refer to
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------