How many USB devices can I theoretically connect to 1788?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How many USB devices can I theoretically connect to 1788?

1,373件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rnassiri on Fri Oct 03 11:06:58 MST 2014
Hi,
Very new at this.
I am trying to choose a micro-controller. Since a USB host theoretically can have 127 devices connected to it, is it fair to conclude the two USBs on a LPC1788 can have 127x2 devices connected to them?

Or does it only support 2 at a time; one for each USB?

I do realize implementing it is a different story.

Thanks.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,366件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rnassiri on Thu Oct 09 13:46:58 MST 2014
Thanks for the link.
It's 127.
0 件の賞賛
返信

1,366件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfb on Thu Oct 09 01:27:23 MST 2014
Download a copy of the NXP LPC178x/7x User manual (UM10470) from:

www.nxp.com/documents/user_manual/UM10470.pdf

Read Chapter 13: LPC178x/7x USB device controller. I'm not a USB expert by any means so can't say for sure but it look like you'll find the answers you are looking for (and a whole lot more) there.
0 件の賞賛
返信