LPC8N04 8Mhz FRO is 2 % accuracy from LPC8N04 spec following.
How about 32khz FRO accuracy? I can't find it in the spec.
Clock generation 8 MHz internal RC oscillator, trimmed to 2 % accuracy, which is used for the system clock Timer oscillator operating at 32 kHz linked to the RTC timer unit
Hello Li-Chin,
We do not have a characterized number, but the accuracy should not be a problem it would be less than 2%
Hope it helps!
Victor.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------