@Victor Jimenez,
Thank you for your information .
I have another concern about IRQ Type ,
In the cmsis_11cxx.h , it define some kinds of interrupt
typedef enum LPC11CXX_IRQn {
NonMaskableInt_IRQn = -14, /*!< 2 Non Maskable Interrupt */
HardFault_IRQn = -13, /*!< 3 Cortex-M0 Hard Fault Interrupt */
SVCall_IRQn = -5, /*!< 11 Cortex-M0 SV Call Interrupt */
PendSV_IRQn = -2, /*!< 14 Cortex-M0 Pend SV Interrupt */
SysTick_IRQn = -1, /*!< 15 Cortex-M0 System Tick Interrupt */
PIO0_0_IRQn = 0, /*!< GPIO port 0, pin 0 Interrupt */
PIO0_1_IRQn = 1, /*!< GPIO port 0, pin 1 Interrupt */
PIO0_2_IRQn = 2, /*!< GPIO port 0, pin 2 Interrupt */
PIO0_3_IRQn = 3, /*!< GPIO port 0, pin 3 Interrupt */
PIO0_4_IRQn = 4, /*!< GPIO port 0, pin 4 Interrupt */
PIO0_5_IRQn = 5, /*!< GPIO port 0, pin 5 Interrupt */
PIO0_6_IRQn = 6, /*!< GPIO port 0, pin 6 Interrupt */
PIO0_7_IRQn = 7, /*!< GPIO port 0, pin 7 Interrupt */
PIO0_8_IRQn = 8, /*!< GPIO port 0, pin 8 Interrupt */
PIO0_9_IRQn = 9, /*!< GPIO port 0, pin 9 Interrupt */
PIO0_10_IRQn = 10, /*!< GPIO port 0, pin 10 Interrupt */
PIO0_11_IRQn = 11, /*!< GPIO port 0, pin 11 Interrupt */
PIO1_0_IRQn = 12, /*!< GPIO port 1, pin 0 Interrupt */
CAN_IRQn = 13, /*!< CAN Interrupt */
SSP1_IRQn = 14, /*!< SSP1 Interrupt */
I2C0_IRQn = 15, /*!< I2C Interrupt */
TIMER_16_0_IRQn = 16, /*!< 16-bit Timer0 Interrupt */
TIMER_16_1_IRQn = 17, /*!< 16-bit Timer1 Interrupt */
TIMER_32_0_IRQn = 18, /*!< 32-bit Timer0 Interrupt */
TIMER_32_1_IRQn = 19, /*!< 32-bit Timer1 Interrupt */
SSP0_IRQn = 20, /*!< SSP0 Interrupt */
UART0_IRQn = 21, /*!< UART Interrupt */
Reserved22_IRQn = 22,
Reserved23_IRQn = 23,
ADC_IRQn = 24, /*!< A/D Converter Interrupt */
WDT_IRQn = 25, /*!< Watchdog timer Interrupt */
BOD_IRQn = 26, /*!< Brown Out Detect(BOD) Interrupt */
Reserved27_IRQn = 27,
EINT3_IRQn = 28, /*!< External Interrupt 3 Interrupt */
EINT2_IRQn = 29, /*!< External Interrupt 2 Interrupt */
EINT1_IRQn = 30, /*!< External Interrupt 1 Interrupt */
EINT0_IRQn = 31, /*!< External Interrupt 0 Interrupt */
} LPC11CXX_IRQn_Type;
so can i know what is different between PIO0_0_IRQn and EINT0_IRQn .
Let say if i want to register interrupt for port 2 pin 10 of chip LPC1115 ,
What type of IRQ should i use ?