Hitex LPC1850 Board with wrong power supply damaged?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hitex LPC1850 Board with wrong power supply damaged?

670件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Fri May 31 00:58:41 MST 2013

Hi everybody,


what happens when supplying the Hitex LPC18xx Board accidently with 9V instead 5V? I've seen no fuse or voltage regulator for the 5V supply which protect the board :-( The 3.3V supply has a voltage regulator but it tolerates max. 6.5V. Now I get the error message "target not debuggable". Have I damaged the Board or is it just in a protection mode? Is it possible to rescue it?


Regards,


Martin

ラベル(1)
0 件の賞賛
返信
0 返答(返信)