Hi,

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi,

1,389 Views
jobin40
Contributor I

HI,

I am developing usb driver for LPC4357.  For the working of UBB0 we need to set PLL0 to 480MHZ. But i do have some problems in setting PLL0. Can anyone help with that?

0 Kudos
Reply
1 Reply

1,264 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jabin Tankachan,

   Please refer to the LPCopen USB sample code to configure the PLL0 480Mhz, you can download the code from this link:

LPCOpen Software for LPC43XX|NXP 

  Please choose the MCB4357 sample code, and refer to the USB sample code, this lpcopen USB sample code also use 480Mhz clock.

Besides, there also a PLL calculation tool for your reference, you can get the data of the PLL register settings.

Audio PLL settings calculation tool | www.LPCware.com 

Wish it helps you!

If you still have problem, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply