Help identify the device Revision

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help identify the device Revision

1,476件の閲覧回数
langhel
Contributor I

I'm working with LPC55S66JBD100 (HLQFP100) like in image but I can't identify it. Is that Revision 0A or 1B ? I suspect it is 0A.

Issue appears when programming an image/application in ISP mode; after reset the device will not enter in ISP mode again.

The programming sequence works fine on S69 revision 1B though with image executing fine.

Secure boot is not enabled and CFPA and CMPA are blank.

Thank you!

LPC55S66JBD100_Cut.jpg

ラベル(2)
0 件の賞賛
返信
1 返信

1,416件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Lucian Anghel 

We can get the silicon revision through chip revision ID and number: SYSCON->DIEID:

pastedImage_3.png

Have a great day,
Jun Zhang
-------------------------------------------------------------------------------

Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信