Having trouble reading pressure sensor using HS-SPI using LPC55S06-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Having trouble reading pressure sensor using HS-SPI using LPC55S06-EVK

22,579件の閲覧回数
pogi_yogi
Contributor II

Hello,

I am a novice just getting my hands into embedded systems for the first time so bare with me... I am tinkering around with pressure sensors, trying to read data using the SPI interface. I am struggling with reading data from the pressure sensor using the HS-SPI (High speed SPI) serial communication peripheral. I have ensured that all the SCK, MISO, PWR, GND, and CS pins have been connected correctly to the evaluation board. I imported one of the SDK examples (spi_HS_LSPI_dma_b2b_transfer_master) to try and read the pressure sensor. The only thing that I changed in the SDK example is the TRANSFER_SIZE variable from 64U to 2U because the size of the pressure data that is coming from the pressure sensor is only 2 bytes; however, when I run the example, the only thing getting printed is 0x00 0x00. I have included attachments of the datasheet for the pressure sensor that I am using as well as the code that I am using to try and read the pressure sensor.

 

Any help with resolving this issue would be appreciated. Additionally, if you have any sources/books/courses/etc. that you could recommend to me for getting into embedded systems/learning the MCUxpresso IDE I would appreciate that too! I'm just getting my foot in the door of this field trying to learn as much as I can.

 

Thank you!!

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

22,549件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you want to use 16 bits data transfer, pls modify it as the following screenshot. Or in the main() to modify.

config->dataWidth =  kSPI_Data16Bits; //kSPI_Data8Bits;

In the main():

SPI_MasterGetDefaultConfig(&masterConfig);
sourceClock = EXAMPLE_SPI_MASTER_CLK_FREQ;
masterConfig.sselNum = (spi_ssel_t)EXAMPLE_SPI_SSEL;
masterConfig.sselPol = (spi_spol_t)EXAMPLE_SPI_SPOL;
masterConfig.dataWidth=kSPI_Data16Bits;
SPI_MasterInit(EXAMPLE_SPI_MASTER, &masterConfig, sourceClock);

 

 

xiangjun_rong_0-1682390032152.png

 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

22,525件の閲覧回数
pogi_yogi
Contributor II
I modified the config->dataWidth to 16 bits in the fsl_spi.c file as you did in the screenshot and I'm still having the same issue reading 0x00 0x00. I also tried doing it in the main() function as you suggested, but still same issue reading 0x00 0x00.
0 件の賞賛
返信

22,480件の閲覧回数
frank_m
Senior Contributor III

Short of reading your datasheet and your code myself ...

Are you sure the SPI settings are correct ?
SPI is not a fixed standard. Endianess, clock polarity and trigger edges may vary, and depend on the slave.
Some slave devices need special treatment. I recently had a device which nominally supported 16-bit transfers, but required a 60ns break between bytes, which required me to break it up into two byte transfers.

I would suggest to take a scope or logic analyzer, and compare your signals carefully with the requirements from the datasheet.

0 件の賞賛
返信

22,468件の閲覧回数
pogi_yogi
Contributor II

From reading the data sheet, it looks like the slave device will send out the most significant bits of the pressure data first, for clock polarity: the clock starts at a low state and becomes active on high, for clock phase: data is read on the clock's first edge, clock frequency should be set in between 50-800 KHz; I have it at 500 KHz. I set all of these in the SPI_MasterGetDefaultConfig function.

 

Attached to this response are images of readings from the oscilloscope. Something odd is that with the high-speed SPI that I'm trying to use, the chip select signal (in purple) never gets pulled down, also the clock signal (in yellow) only oscillates up to ~1.5V, and the MISO signal (in blue) just alternates between 1 and 0. 

 

I ran an example using the "normal" SPI using FLEXCOMM3, and it was able to work just fine. If you look at the attached image, you can see the chip select signal getting pulled down, the clock oscillating from 0V to 3V, and the MISO signal producing reasonable signals besides just alternating between 1 and 0. 

 

I do not know why the high-speed SPI signal is behaving in such an odd way.

0 件の賞賛
返信

22,488件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you connect the /CS, SCK and MISO signals to scope and check if there is output data from temperature sensor  on the MISO pin.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

22,467件の閲覧回数
pogi_yogi
Contributor II
Hi xiangjun_rong, please view my response to frank_meyer above. It has details about the scope signals and images attached.

Thank you!
0 件の賞賛
返信

22,456件の閲覧回数
frank_m
Senior Contributor III

Keep in mind that SPI is a digital signal, requiring about one order of magnitude higher bandwidth of the lines than the SCLK frequency. And you need to keep the wires/connections/PCB traces reasonable short.
Albeit below 1MHz, termination resistors are usually not necessary.
The wave shape of the "high-speed" SCLK signal looks ok, the amplitude not. But such an attenuation would be unreasonable below the specified clock limit.
Are you sure the scaling of the scope channels is the same ?

Have you checked the SS signal is correct, and does not assert before the transmission is complete ?

 

 

0 件の賞賛
返信