Having Problem working on SPI...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Having Problem working on SPI...

1,447件の閲覧回数
nisargnyk
Contributor I

I am working on LPC1768, Interfaced with CS5463.

Getting Clock and MOSI pulses of 3.3V even making it open drain, As of my knowledge CS5463 needs Pulses having 4.8V for High Logic, Alias I am getting to 3.3V only That is why my SPI is malfunctioning, Readings are not stable and even not precised..

So how can i get upto 5V pulses from SPI pins.

Regards Nisarg.

ラベル(2)
0 件の賞賛
返信
1 返信

1,327件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Nisarg,

I copy part of the data sheet of CS5463, from the description, the VA+ is 5V, but the VD+ can be from 3.3V to 5V, I suggest you connect 3.3V power supply to VD+ pin, in this way, all digital logic will be 3.3V, it is easy for the the LPC1768 to interface with.

If you do want to connect VD+ to 5V power supply, I suppose that a transceiver chip is required, one side is 5V, another side is 3.3V.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png