Hardfault during Expedited access using LPC CANAPI with -Os compiler optimization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hardfault during Expedited access using LPC CANAPI with -Os compiler optimization

1,769件の閲覧回数
raphaelmeyer
Contributor I

Morning!

I'm implementing currently a firmware for a LPC11C14 MCU which should communicate with other nodes over CANopen.

Since the chip provides a CANopen API in its ROM, I decided to use it for my purpose according to the App note AN11238, LPC11Cxx CANopen network demo. Everything works fine so far as long as I compile the code with either the optimization -Od or -O1 to -O3. As soon as I compile the code with optimization for size activated (-Os), I get a hardfault during a CANopen Expedited request, segmented access works fine still. The hardfault even occurs when the callback function for the reqeusts is totally empty. Timingwise, the callback "CANopen_SDOS_Exp_Write" and "CANopen_SDOS_Exp_Read" is called correctly and returns normally. After the return of the callback, the MCU crashes.

 

Attached the code of the canopen library I'm using. Most parts are taken from the Appnote's driver, just some defines for better readability have been added as well as a method for adding entries to the object dictionary before the start of the CAN interface. Further, I attached the linker scripts.

Any ideas?

 

Regards, Raphael

Original Attachment has been moved to: canopen.h.zip

Original Attachment has been moved to: ldscripts.zip

Original Attachment has been moved to: can_node_sdo.c.zip

Original Attachment has been moved to: can_node_sdo.h.zip

Original Attachment has been moved to: canopen.c.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,510件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Could you please confirm the IDE you are using? 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信