HID USB ROM Driver LPC11U24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HID USB ROM Driver LPC11U24

1,121件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tanyashir on Wed Jan 30 12:35:12 MST 2013
Hello!

I use HID USB ROM Driver of LPC11U24. I have download examples archive from this link: http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc11uxx-peripherals-using-lpcxpresso and I have used example named  “USB_ROM_HID” from archive.

This example works. But there is a problem that it sends data with specified intervals. Even if I write zero size of sending bytes to the endpoint, the report goes to the computer, in which the number of bytes is zero.

How can I do so that data are sending only when I need it?
ラベル(1)
0 件の賞賛
返信
0 返答(返信)