Getting started with LPC1778FBD208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting started with LPC1778FBD208

Jump to solution
2,955 Views
aus_swsol
Contributor I

Hi Expert,

Im using LPC1778FBD208 with 208 pin numbers. Im using pin 59 to blink LED.

Currenlty using Keil IDE and managed to works on GD32 MCU. Can you guide me how to build in project for LPC in Keil. Im very appreciate if you can share me the full project sdk. I just need to open, build & flash. Im using CMSIS-DAP to flash the code.

Thanks in advanced.

0 Kudos
Reply
1 Solution
2,750 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @aus_swsol 

Sorry, we have reported the download issue to our website team and will resolve it as soon as possible so that you can download the resources.

BR

Harry

View solution in original post

0 Kudos
Reply
6 Replies
2,938 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @aus_swsol 

You can access to the NXP lpcopen website

LPCOpen Software for LPC17XX | NXP Semiconductors

And download the lpc1788 Keil packet.

Harry_Zhang_0-1736494230165.png

You can modify the project according to your needs based on this Keil project.

BR

Harry

0 Kudos
Reply
2,929 Views
aus_swsol
Contributor I

*additional reply

other problem:-

1) the LED to blink also was wrong. below is my code, but the LED that blink is at P2[27] which is pin 47. i want to blink led at P2[18] which is pin 59.

aus_swsol_0-1736501741372.png

2) i need to enter debug mode, run debug mode. then  exit the debug mode to make it run. why? if i reset power, the board doesnt blink pin 47.

 

thanks in advanced

 

0 Kudos
Reply
2,935 Views
aus_swsol
Contributor I

Hi Harry,

This is what happened when I clicked

aus_swsol_0-1736496629604.png

Can you please provide me the latest stable SDK with example for LPC1778FBD208?

Im using Keil. currently my solution is using the library from this github. Im not sure this is official stable version or not.
https://github.com/openxc/nxp-cdl/tree/master

 

Lib I used was from these two folder and managed to blink the LED.

CMSISv2p00_LPC177x_8x

LPC177x_8xLib

However, I need a full example for these library to fast plot my project.

 

Thanks in advanced

 

0 Kudos
Reply
2,880 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @aus_swsol 

Sorry, our LPCopen official website has some issues, we will resolve this problem as soon as possible.

https://github.com/openxc/nxp-cdl/tree/master

This code is not officially maintained by us.

So I still suggest that you import keil examples from LPCopen.

BR

Harry

0 Kudos
Reply
2,856 Views
aus_swsol
Contributor I

Hi Harry,

Kindly please attach KEIL project with example using LPC1778FBD208 CMSIS & standard library for me to get startup with.

Thanks in advanced.

0 Kudos
Reply
2,750 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @aus_swsol 

Sorry, we have reported the download issue to our website team and will resolve it as soon as possible so that you can download the resources.

BR

Harry

0 Kudos
Reply