GPIO Interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO Interrupts

1,039件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Wed Aug 28 07:55:34 MST 2013
Hello,

I want to configure / enable GPIO Interrupt.
I've noticed there are no CHIP methods, but only IP methods for GPIO Interrupt.

Strangely enough the IP methods are defined in gpioint_001.h BUT this is never included anywhere!
Why is it not one of the 'Chip layer required IP layer drivers'?

Why is it not included in any of the lpc_core header files?

Any help is greatly appreciated!

ラベル(1)
0 件の賞賛
返信
0 返答(返信)