GPIO Interrupts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO Interrupts

1,038 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Wed Aug 28 07:55:34 MST 2013
Hello,

I want to configure / enable GPIO Interrupt.
I've noticed there are no CHIP methods, but only IP methods for GPIO Interrupt.

Strangely enough the IP methods are defined in gpioint_001.h BUT this is never included anywhere!
Why is it not one of the 'Chip layer required IP layer drivers'?

Why is it not included in any of the lpc_core header files?

Any help is greatly appreciated!

Labels (1)
0 Kudos
Reply
0 Replies