GINT中断失效问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GINT中断失效问题

4,054件の閲覧回数
lizhihong
Contributor III

GINT中断失效时序图.jpg

GINT使用边沿方式“或”运算过程中有疑问,请解答一下,谢谢。

GINT初始化2个以上引脚为同一组中断,图上举例为2个引脚为一组,且经过实测现象绘制。

当同组中无任一极性有效的信号时,任意一个引脚产生极性有效信号,则产生中断,这个可以理解;

同组中有任一极性有效的信号时,任意一个引脚产生极性有效信号,也不产生中断,这个我无法理解。

当运用到实际当中时,我可能会在图上虚线指示位置进入POWERDOWN低功耗模式,只允许GINT唤醒,而不允许PINT唤醒。

如果此时有一个信号一直处于极性有效时进入低功耗,则同组内其他引脚的极性有效信号均无法唤醒MCU,导致低功耗下睡死。特别是外接模块的中断信号为电平信号,且电平中断信号需要MCU唤醒之后处理才能清除的情况下,有较大概率复现。

目前我的硬件设计当中存在较多的电平中断信号,其中有2个需要MCU唤醒后处理来清除,还有2个是外接输入的电平中断信号,MCU无法控制清除,剩下的均为边沿信号。

如果使用电平中断方式,由于进入中断非常频繁,会导致无法运行中断服务函数以外的函数。

因此,希望能提供一个可靠的方法,在POWERDOWN模式下,使用电平信号唤醒MCU。

开发环境:

keil 5.29

keil  DFP pack 12.1.0

KSDK 2.7.0

driver_example: power_manager_lpc

ラベル(2)
タグ(2)
0 件の賞賛
返信
9 返答(返信)

2,951件の閲覧回数
daweiyou
NXP Employee
NXP Employee

虽然时间久了,但是我还是想回复下这个问题的解法:

1.GINT有两组,可以将两个信号分配到两个GINT上面;

2.GINT的edge和level都是指的信号产生之后的结果是edge还是level,对于io应该都是level,这个也符合GINT能在power down模式下使用的特性;

3.如(2)所述,遇到在虚线处要进入休眠,而且只使用一个GINT的场合,应该读取两个pin的状态,实时调整Pa-b的触发电平,再进入休眠。

0 件の賞賛
返信

3,795件の閲覧回数
francisy
Contributor II

I have the similar issue before. I switch to use libpower_softabi.a instead of libpower_hardabi.a, then it works again. And then I switch back to libpower_hardabi.a it also works. I understand it seems make no sense. But you may have a try.

0 件の賞賛
返信

3,795件の閲覧回数
lizhihong
Contributor III

Actually, I'm not confused about the libpower built by hardabi or softabi option.

It's about interrupt functions of the GPIOs configured in GINT(it's few description in UM11126.pdf), whether GINT is used in lowpower or not。

Thank you.

0 件の賞賛
返信

3,795件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

非常感谢使用NXP产品,很高兴为你提供技术支持!
诚如你所说,如果GINT的中断触发表现如你所言,我觉得你可以考虑PINT中断来用于唤醒MCU。

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,795件の閲覧回数
lizhihong
Contributor III

这项目如果无法规避“低功耗唤醒失效”这种情况,就会卡在这里无法实现量产,很有可能就流产了。

麻烦帮忙再分析分析,非常感谢!!!

deep sleep; power-down; deep power-down 这3种低功耗模式的选择。

基于功耗、唤醒引脚数量、唤醒是否复位、唤醒时间考虑:

  • 选择了power-down模式。功耗全SRAM保持典型值15.4uA,唤醒引脚为GINT包含的所有引脚,但不支持PINT,唤醒不复位,唤醒时间346us;
  • pass了deep power-down模式,不支持GINT、PINT唤醒,且最多只有4个wakeup pins,我需要6~8个,且唤醒后会复位;
  • pass了deep-sleep模式,支持GINT、PINT唤醒,但功耗过高。

pastedImage_5.png

pastedImage_6.png

pastedImage_3.png唤醒源1.jpg唤醒源2.jpg

pastedImage_4.png

0 件の賞賛
返信

3,795件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

根据你的介绍,项目中选择power-down模式作为要进入的低功耗模式,但是根据你实际的测试,GINT中断触发呈现如下的形式,不太满足目前的需求。

我这边已帮你在分析,看看基于LPC55S69还有没有其他资源可以利用。

GINT中断失效时序图.jpg

GINT使用边沿方式“或”运算过程中有疑问,请解答一下,谢谢。

GINT初始化2个以上引脚为同一组中断,图上举例为2个引脚为一组,且经过实测现象绘制。

当同组中无任一极性有效的信号时,任意一个引脚产生极性有效信号,则产生中断,这个可以理解;

当同组中有任一极性有效的信号时,任意一个引脚产生极性有效信号,也不产生中断,这个我无法理解。

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,795件の閲覧回数
lizhihong
Contributor III

The reason why GINT interrupt request is not created, I speculate:

A new interrupt request will not creat untill the interrupt request signal dissipate. Even though, interrupt request has been deal with headler function.

0 件の賞賛
返信

3,795件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi

Thanks for your reply.
In theory, after the code handling the edge-sensitive interrupt, the level of voltage won't raise an interrupt again.

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,795件の閲覧回数
lizhihong
Contributor III
/*
 * Copyright (c) 2016, Freescale Semiconductor, Inc.
 * Copyright 2016-2019 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

#include "fsl_debug_console.h"
#include "board.h"
#include "fsl_common.h"
#include "fsl_power.h"
#include "fsl_inputmux.h"
#include "fsl_pint.h"
#include "fsl_usart.h"
#if (defined(FSL_FEATURE_POWERLIB_EXTEND) && FSL_FEATURE_POWERLIB_EXTEND)
#include "fsl_gint.h"
#endif

#include "pin_mux.h"
#include "fsl_rtc.h"
#include <stdbool.h>
/*******************************************************************************
 * Definitions
 ******************************************************************************/
#define DEMO_WAKEUP_WITH_GINT (1)
#define APP_USART_RX_ERROR kUSART_RxError
#define APP_RUNNING_INTERNAL_CLOCK BOARD_BootClockFRO12M()
#define APP_USER_WAKEUP_KEY3_NAME "SW3"
#define APP_USER_WAKEUP_KEY3_GPIO BOARD_SW3_GPIO
#define APP_USER_WAKEUP_KEY3_PORT BOARD_SW3_GPIO_PORT
#define APP_USER_WAKEUP_KEY3_PIN BOARD_SW3_GPIO_PIN
#define APP_USER_WAKEUP_KEY3_INPUTMUX_SEL kINPUTMUX_GpioPort1Pin9ToPintsel
#define APP_USER_WAKEUP_KEY2_NAME "SW2"
#define APP_USER_WAKEUP_KEY2_GPIO BOARD_SW2_GPIO
#define APP_USER_WAKEUP_KEY2_PORT BOARD_SW2_GPIO_PORT
#define APP_USER_WAKEUP_KEY2_PIN BOARD_SW2_GPIO_PIN
#define APP_USER_WAKEUP_KEY2_INPUTMUX_SEL kINPUTMUX_GpioPort1Pin18ToPintsel

#define DEMO_GINT0_PORT kGINT_Port1
#define DEMO_GINT1_PORT kGINT_Port1

/* Select one input, active low for GINT0 */
#define DEMO_GINT0_POL_MASK ~(1U << BOARD_SW3_GPIO_PIN)
#define DEMO_GINT0_ENA_MASK (1U << BOARD_SW3_GPIO_PIN)

/* Select two inputs, active low for GINT1. SW2 & SW3 must be connected to the same port */
#define DEMO_GINT1_POL_MASK ~((1U << BOARD_SW2_GPIO_PIN) )
#define DEMO_GINT1_ENA_MASK ((1U << BOARD_SW2_GPIO_PIN) )

#define APP_EXCLUDE_FROM_SLEEP (kPDRUNCFG_PD_LDOMEM | kPDRUNCFG_PD_LDODEEPSLEEP)

#define APP_EXCLUDE_FROM_DEEPSLEEP (kPDRUNCFG_PD_DCDC | kPDRUNCFG_PD_FRO192M | kPDRUNCFG_PD_FRO32K)

#define APP_EXCLUDE_FROM_POWERDOWN (kPDRUNCFG_PD_LDOMEM | kPDRUNCFG_PD_FRO32K)

#define APP_EXCLUDE_FROM_DEEPPOWERDOWN (kPDRUNCFG_PD_LDOMEM | kPDRUNCFG_PD_FRO32K)

#define APP_SYSCON_STARTER_MASK SYSCON_STARTERSET_GPIO_INT00_SET_MASK
//#define INPUTMUX INPUTMUX0
const char *gWakeupInfoStr[] = {"Sleep [Press the user key to wakeup]""Deep Sleep [Press the user key to wakeup]",
#if (defined(FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE) && FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE)
                                "Powerdown [Reset to wakeup]""Deep Powerdown [Reset to wakeup]"};
#else
                                "Deep Powerdown [Reset to wakeup]""Deep Powerdown [Reset to wakeup]"};
#endif
uint32_t gCurrentPowerMode;

/*******************************************************************************
 * Prototypes
 ******************************************************************************/
void DEMO_PreLowPower(void);
void DEMO_PowerDownWakeup(void);
void DEMO_PreDeepPowerDown(void);
static uint32_t APP_GetUserSelection(void);
static void APP_InitWakeupPin(void);
static void pint_intr_callback(pint_pin_int_t pintr, uint32_t pmatch_status);

/*******************************************************************************
 * Code
 ******************************************************************************/
void RTC_IRQHandler(void)
{
}
void DEMO_PreLowPower(void)
{
    /*!< Configure RTC OSC */
    POWER_EnablePD(kPDRUNCFG_PD_XTAL32K); /*!< Powered down the XTAL 32 kHz RTC oscillator */
    POWER_DisablePD(kPDRUNCFG_PD_FRO32K); /*!< Powered the FRO 32 kHz RTC oscillator */
    CLOCK_AttachClk(kFRO32K_to_OSC32K);   /*!< Switch OSC32K to FRO32K */

    CLOCK_SetFLASHAccessCyclesForFreq(32768U); /*!< Set FLASH wait states for core */

    /*!< Set up dividers */
    CLOCK_SetClkDiv(kCLOCK_DivAhbClk, 1Ufalse); /*!< Set AHBCLKDIV divider to value 1 */

    /*!< Set up clock selectors - Attach clocks to the peripheries */
    CLOCK_AttachClk(kOSC32K_to_MAIN_CLK); /*!< Switch MAIN_CLK to OSC32K */

    /*< Set SystemCoreClock variable. */
    SystemCoreClock = 32768U;
}
void DEMO_PowerDownWakeup(void)
{
    BOARD_BootClockFRO12M();
    BOARD_InitDebugConsole();
}
void DEMO_PreDeepPowerDown(void)
{
    uint32_t sec = 0;
    uint32_t currSeconds;
    uint8_t index = 0;
    rtc_datetime_t date;

    /* Set a start date time and start RT */
    date.year   = 2018U;
    date.month  = 12U;
    date.day    = 25U;
    date.hour   = 19U;
    date.minute = 0;
    date.second = 0;

    /* Get alarm time from user */
    PRINTF("Please input the number of second to wait for waking up\r\n");
    PRINTF("The second must be positive value\r\n");
    while (index != 0x0D)
    {
        index = GETCHAR();
        if ((index >= '0') && (index <= '9'))
        {
            PUTCHAR(index);
            sec = sec * 10 + (index - 0x30U);
        }
    }
    PRINTF("\r\n");

    POWER_EnablePD(kPDRUNCFG_PD_XTAL32K); /*!< Powered down the XTAL 32 kHz RTC oscillator */
    POWER_DisablePD(kPDRUNCFG_PD_FRO32K); /*!< Powered the FRO 32 kHz RTC oscillator */
    CLOCK_AttachClk(kFRO32K_to_OSC32K);   /*!< Switch OSC32K to FRO32K */

    CLOCK_SetFLASHAccessCyclesForFreq(32768U); /*!< Set FLASH wait states for core */

    /*!< Set up dividers */
    CLOCK_SetClkDiv(kCLOCK_DivAhbClk, 1Ufalse); /*!< Set AHBCLKDIV divider to value 1 */

    /*!< Set up clock selectors - Attach clocks to the peripheries */
    CLOCK_AttachClk(kOSC32K_to_MAIN_CLK); /*!< Switch MAIN_CLK to OSC32K */

    /*< Set SystemCoreClock variable. */
    SystemCoreClock = 32768U;

    /* Init RTC */
    RTC_Init(RTC);

    /* RTC time counter has to be stopped before setting the date & time in the TSR register */
    RTC_StopTimer(RTC);

    /* Set RTC time to default */
    RTC_SetDatetime(RTC, &date);

    /* Enable RTC alarm interrupt */
    RTC_EnableInterrupts(RTC, kRTC_AlarmInterruptEnable);

    /* Enable at the NVIC */
    EnableIRQ(RTC_IRQn);

    /* Start the RTC time counter */
    RTC_StartTimer(RTC);

    /* Read the RTC seconds register to get current time in seconds */
    currSeconds = RTC->COUNT;

    /* Add alarm seconds to current time */
    currSeconds += sec;

    /* Set alarm time in seconds */
    RTC->MATCH = currSeconds;

    /* Get alarm time */
    RTC_GetAlarm(RTC, &date);

    PRINTF("System will wakeup at%02ds later\r\n"date.second);
}
/*!
 * @brief Main function
 */
int main(void)
{
    /* Init board hardware. */
    CLOCK_EnableClock(kCLOCK_Gpio0); /* Enable the clock for GPIO0. */

    /* attach 12 MHz clock to FLEXCOMM0 (debug console) */
    CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);

    BOARD_InitBootPins();
    manage_evk_io_optimization();
    BOARD_BootClockPLL150M();
    BOARD_InitDebugConsole();

    /* Running 12 MHz to Core*/
    APP_RUNNING_INTERNAL_CLOCK;

    /* Attach Main Clock as CLKOUT */
    CLOCK_AttachClk(kMAIN_CLK_to_CLKOUT);

    APP_InitWakeupPin();

    PRINTF("Power Manager Demo for LPC device.\r\n");
    PRINTF("The \"user key\" is: %s\r\n", APP_USER_WAKEUP_KEY3_NAME);
    PRINTF("The \"user key\" is: %s\r\n", APP_USER_WAKEUP_KEY2_NAME);

    while (1)
    {
        gCurrentPowerMode = APP_GetUserSelection();
        PRINTF("Entering %s ...\r\n"gWakeupInfoStr[gCurrentPowerMode]);

        /* Enter the low power mode. */
        switch (gCurrentPowerMode)
        {
            case kPmu_Sleep: /* Enter sleep mode. */
                POWER_EnterSleep();
                break;
            case kPmu_Deep_Sleep: /* Enter deep sleep mode. */
#if (defined(FSL_FEATURE_POWERLIB_EXTEND) && FSL_FEATURE_POWERLIB_EXTEND)
                POWER_EnterDeepSleep(APP_EXCLUDE_FROM_DEEPSLEEP, 0x0, WAKEUP_GPIO_INT0_0, 0x0);
#else
                POWER_EnterDeepSleep(APP_EXCLUDE_FROM_DEEPSLEEP);
#endif
                break;
#if (defined(FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE) && FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE)
            case kPmu_PowerDown: /* Enter power down mode. */
                PRINTF(
                    "Press any key to confirm to enter the power down mode and wakeup the device by press s1 key on "
                    "board.\r\n\r\n");
                GETCHAR();

#if (defined(FSL_FEATURE_POWERLIB_EXTEND) && FSL_FEATURE_POWERLIB_EXTEND)
#if (defined(DEMO_WAKEUP_WITH_GINT) && DEMO_WAKEUP_WITH_GINT)
                DEMO_PreLowPower();
                POWER_EnterPowerDown(APP_EXCLUDE_FROM_POWERDOWN, 0x7FFF,
                                     WAKEUP_GPIO_GLOBALINT0 | WAKEUP_GPIO_GLOBALINT1, 1);
                DEMO_PowerDownWakeup();
                APP_InitWakeupPin();
#endif
#else
                POWER_EnterPowerDown(APP_EXCLUDE_FROM_POWERDOWN);
#endif
                break;
#endif
            case kPmu_Deep_PowerDown: /* Enter deep power down mode. */
                PRINTF(
                    "Press any key to confirm to enter the deep power down mode and wakeup the device by "
                    "reset.\r\n\r\n");
                GETCHAR();
#if (defined(FSL_FEATURE_POWERLIB_EXTEND) && FSL_FEATURE_POWERLIB_EXTEND)
                DEMO_PreDeepPowerDown();
                POWER_EnterDeepPowerDown(APP_EXCLUDE_FROM_DEEPPOWERDOWN,
                                         LOWPOWER_SRAMRETCTRL_RETEN_RAMX2 | LOWPOWER_SRAMRETCTRL_RETEN_RAMX3,
                                         WAKEUP_RTC_LITE_ALARM_WAKEUP, 1);
#else
                POWER_EnterDeepPowerDown(APP_EXCLUDE_FROM_DEEPSLEEP);
#endif
                break;
            default:
                break;
        }

        PRINTF("Wakeup.\r\n\r\n");
    }
}

#if (defined(DEMO_WAKEUP_WITH_GINT) && DEMO_WAKEUP_WITH_GINT)
/*!
 * @brief Call back for GINT0 event
 */
void gint0_callback(void)
{
    PRINTF("\r\nGin0 event occurs\r\n");
}
/*!
 * @brief Call back for GINT1 event
 */
void gint1_callback(void)
{
    PRINTF("\r\nGin1 event occurs\r\n");
}
#endif

/*
 * Setup a GPIO input pin as wakeup source.
 */
static void APP_InitWakeupPin(void)
{
    gpio_pin_config_t gpioPinConfigStruct;

    /* Set SW pin as GPIO input. */
    gpioPinConfigStruct.pinDirection = kGPIO_DigitalInput;
    GPIO_PinInit(APP_USER_WAKEUP_KEY3_GPIO, APP_USER_WAKEUP_KEY3_PORT, APP_USER_WAKEUP_KEY3_PIN, &gpioPinConfigStruct);

    /* Configure the Input Mux block and connect the trigger source to PinInt channle. */
    INPUTMUX_Init(INPUTMUX);
    INPUTMUX_AttachSignal(INPUTMUX, kPINT_PinInt0, APP_USER_WAKEUP_KEY3_INPUTMUX_SEL); /* Using channel 0. */
    INPUTMUX_Deinit(INPUTMUX); /* Turnoff clock to inputmux to save power. Clock is only needed to make changes */

    /* Set SW pin as GPIO input. */
    gpioPinConfigStruct.pinDirection = kGPIO_DigitalInput;
    GPIO_PinInit(APP_USER_WAKEUP_KEY2_GPIO, APP_USER_WAKEUP_KEY2_PORT, APP_USER_WAKEUP_KEY2_PIN, &gpioPinConfigStruct);

    /* Configure the Input Mux block and connect the trigger source to PinInt channle. */
    INPUTMUX_Init(INPUTMUX);
    INPUTMUX_AttachSignal(INPUTMUX, kPINT_PinInt0, APP_USER_WAKEUP_KEY3_INPUTMUX_SEL); /* Using channel 0. */
    INPUTMUX_Deinit(INPUTMUX); /* Turnoff clock to inputmux to save power. Clock is only needed to make changes */

#if !(defined(FSL_FEATURE_POWERLIB_EXTEND) && FSL_FEATURE_POWERLIB_EXTEND)
    /* Enable wakeup for PinInt0. */
    SYSCON->STARTERSET[0] |= APP_SYSCON_STARTER_MASK; /* GPIO pin interrupt 0 wake-up. */
#endif

//    /* Configure the interrupt for SW pin. */
//    PINT_Init(PINT);
//    PINT_PinInterruptConfig(PINT, kPINT_PinInt0, kPINT_PinIntEnableFallEdge, pint_intr_callback);
//    PINT_EnableCallback(PINT); /* Enable callbacks for PINT */

#if !(defined(FSL_FEATURE_POWERLIB_EXTEND) && FSL_FEATURE_POWERLIB_EXTEND)
    EnableDeepSleepIRQ(PIN_INT0_IRQn);
#endif
//#if (defined(DEMO_WAKEUP_WITH_GINT) && DEMO_WAKEUP_WITH_GINT)
//    /* Initialize GINT0*/
//    GINT_Init(GINT0);

//    /* Setup GINT0 for edge trigger, "OR" mode */
//    GINT_SetCtrl(GINT0, kGINT_CombineOr, kGINT_TrigEdge, gint0_callback);

//    /* Select pins & polarity for GINT0 */
//    GINT_ConfigPins(GINT0, DEMO_GINT0_PORT, DEMO_GINT0_POL_MASK, DEMO_GINT0_ENA_MASK);

//    /* Enable callbacks for GINT0 & GINT1 */
//    GINT_EnableCallback(GINT0);
//#endif

    /* Initialize GINT0 & GINT1 */
    GINT_Init(GINT0);

#if defined(FSL_FEATURE_SOC_GINT_COUNT) && (FSL_FEATURE_SOC_GINT_COUNT > 1)
    GINT_Init(GINT1);
#endif

    /* Setup GINT0 for edge trigger, "OR" mode */
    GINT_SetCtrl(GINT0, kGINT_CombineOr, kGINT_TrigLevel, gint0_callback);

/* Setup GINT1 for edge trigger, "AND" mode */
#if defined(FSL_FEATURE_SOC_GINT_COUNT) && (FSL_FEATURE_SOC_GINT_COUNT > 1)
//    GINT_SetCtrl(GINT1, kGINT_CombineAnd, kGINT_TrigEdge, gint1_callback);
    GINT_SetCtrl(GINT1, kGINT_CombineOr, kGINT_TrigEdge, gint1_callback);

#endif
    /* Select pins & polarity for GINT0 */
    GINT_ConfigPins(GINT0, DEMO_GINT0_PORT, DEMO_GINT0_POL_MASK & DEMO_GINT1_POL_MASK, DEMO_GINT0_ENA_MASK | DEMO_GINT1_ENA_MASK);

    /* Select pins & polarity for GINT1 */

#if defined(FSL_FEATURE_SOC_GINT_COUNT) && (FSL_FEATURE_SOC_GINT_COUNT > 1)
    GINT_ConfigPins(GINT1, DEMO_GINT1_PORT, DEMO_GINT0_POL_MASK & DEMO_GINT1_POL_MASK, DEMO_GINT0_ENA_MASK | DEMO_GINT1_ENA_MASK);
#endif
    /* Enable callbacks for GINT0 & GINT1 */
    GINT_EnableCallback(GINT0);

#if defined(FSL_FEATURE_SOC_GINT_COUNT) && (FSL_FEATURE_SOC_GINT_COUNT > 1)
    GINT_EnableCallback(GINT1);
#endif

}

/*
 * Callback function when wakeup key is pressed.
 */
static void pint_intr_callback(pint_pin_int_t pintr, uint32_t pmatch_status)
{
    PRINTF("Pin event occurs\r\n");
}

/*
 * Get user selection from UART.
 */
static uint32_t APP_GetUserSelection(void)
{
    uint32_t ch;

    /* Clear rx overflow error once it happens during low power mode. */
    if (APP_USART_RX_ERROR == (APP_USART_RX_ERROR & USART_GetStatusFlags((USART_Type *)BOARD_DEBUG_UART_BASEADDR)))
    {
        USART_ClearStatusFlags((USART_Type *)BOARD_DEBUG_UART_BASEADDR, APP_USART_RX_ERROR);
    }

    PRINTF(
        "Select an option\r\n"
        "\t1. Sleep mode\r\n"
        "\t2. Deep Sleep mode\r\n"
#if (defined(FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE) && FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE)
        "\t3. power down mode\r\n"
        "\t4. Deep power down mode\r\n");
#else
        "\t3. Deep power down mode\r\n");
#endif
    while (1)
    {
        ch = GETCHAR();
#if (defined(FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE) && FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE)
        if ((ch < '1') || (ch > '4')) /* Only '1', '2', '3' , '4'. */
#else
        if ((ch < '1') || (ch > '3')) /* Only '1', '2', '3'. */
#endif
        {
            continue;
        }
        else
        {
            ch = ch - '1'/* Only 0, 1, 2 (,3). */
            break;
        }
    }
    switch (ch)
    {
        case 0:
            ch = kPmu_Sleep;
            break;
        case 1:
            ch = kPmu_Deep_Sleep;
            break;
#if (defined(FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE) && FSL_FEATURE_SYSCON_HAS_POWERDOWN_MODE)
        case 2:
            ch = kPmu_PowerDown;
            break;
        case 3:
            ch = kPmu_Deep_PowerDown;
            break;
#else
        case 2:
            ch = kPmu_Deep_PowerDown;
            break;
#endif
    }
    return ch;
}
0 件の賞賛
返信