Function returning wrong value in lpc824

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Function returning wrong value in lpc824

1,588 Views
johnygeorgemala
Contributor I

I am working on porting an application running on `Arduino Mega` to `LPC824`.

The following piece of code is working differently for both the platforms.

/** * Calculation of CMAC */ void cmac(const uint8_t* data, uint8_t dataLength) { uint8_t trailer[1] = {0x80}; uint8_t bytes[_lenRnd]; uint8_t temp[_lenRnd]; memcpy(temp, data, dataLength); concatArray(temp, dataLength, trailer, 1); dataLength ++; addPadding(temp, dataLength); memcpy(bytes, _sk2, _lenRnd); xorBytes(bytes,temp,_lenRnd); aes128_ctx_t ctx; aes128_init(_sessionkey, &ctx); uint8_t* chain = aes128_enc_sendMode(bytes, _lenRnd, &ctx, _ivect); Board_UARTPutSTR("chain\n\r"); printBytes(chain, 16, true); memcpy(_ivect, chain, _lenRnd); //memcpy(_ivect, aes128_enc_sendMode(bytes,_lenRnd,&ctx,_ivect), _lenRnd); memcpy(_cmac,_ivect, _lenRnd); Board_UARTPutSTR("Initialization vector\n\r"); printBytes(_ivect, 16, true); }

I am expecting a value like `{0x5d, 0xa8, 0x0f, 0x1f, 0x1c, 0x03, 0x7f, 0x16, 0x7e, 0xe5, 0xfd,

0xf3, 0x45, 0xb7, 0x73, 0xa2}` for the `chain` variable.

But the follow function is working differently. The print inside the function has

the correct value which I want `({5d, 0xa8, 0x0f, 0x1f, 0x1c, 0x03, 0x7f, 0x16,

0x7e, 0xe5, 0xfd, 0xf3, 0x45, 0xb7, 0x73, 0xa2})`.

But when the function returns `chain` is having a different value, compared to what I

am expecting, I get the following value for `chain`

`{0x00, 0x20, 0x00, 0x10, 0x03, 0x01, 0x00, 0x00, 0xd5, 0x00, 0x00, 0x00, 0xd7, 0x00, 0x00, 0x00}`

Inside the function, the result is correct. But it returns a wrong value to the

function which called it. Why is it happening so ?

uint8_t* aes128_enc_sendMode(unsigned char* data, unsigned short len, aes128_ctx_t* key, const unsigned char* iv) { unsigned char tmp[16]; uint8_t chain[16]; unsigned char c; unsigned char i; memcpy(chain, iv, 16); while (len >= 16) { memcpy(tmp, data, 16); //xorBytes(tmp,chain,16); for (i = 0; i < 16; i++) { tmp[i] = tmp[i] ^ chain[i]; } aes128_enc(tmp, key); for (i = 0; i < 16; i++) { //c = data[i]; data[i] = tmp[i]; chain[i] = tmp[i]; } len -= 16; data += 16; } Board_UARTPutSTR("Chain!!!:"); printBytes(chain, 16, true); return chain; }

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,453 Views
lpcxpresso_supp
NXP Employee
NXP Employee

So you appear to be trying to return a pointer to a local array (so on the stack). Thus once you have returned from this function,  those values could very easily be overwritten by anything else using the stack (for instance an interrupt being triggered).

Regards,

LPCXpresso Support

0 Kudos
Reply