For LPC-LINK of LPCX_PressoLPC1769

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

For LPC-LINK of LPCX_PressoLPC1769

4,946 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by apollo21 on Mon Dec 17 23:20:00 MST 2012
Greetings
I have two problems.
1, pliers work, the project, if you accidentally delete, and import them again, the imported project, because it remains in the workbench, I can not be imported.
It can not be seen and can not access.
Write a program by connecting the 2, LPC-LINK,
If you try to re-write another program, lose sight of the LPC-LINK, but I can not find any search.
Error of something out and disconnect the USB plug at a time, followed by detecting the LPC-LINK, you can continue to write.
By doing what you can do even if not disconnect the USB (for example, by pressing a push-button switch), continue to write, for example?
Can you more automatically, to avoid the errors that can not be detected or LPC-LINK?
Best regards
apollo21
标签 (1)
0 项奖励
回复
3 回复数

4,912 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Dec 22 10:34:00 MST 2012
Answered in http://knowledgebase.nxp.com/showthread.php?p=20605
0 项奖励
回复

4,912 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by apollo21 on Sat Dec 22 06:38:55 MST 2012
Greetings
I was able to take out from the library "RDB1768cmsis2_uIP" I want to compile.
To pilot Next, check the MAC address and the Ethernet address, "192.168.0.24" IP address, MAC address is displayed as "00-ff-ff-ff-ff-ff".
How do, I will be able to change the MAC address?
Best regards
0 项奖励
回复

4,912 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Daniel Widyanto on Wed Dec 19 00:13:04 MST 2012
Hi,

This is forum for microcontrollers, not the compilers / IDE / etc. Please forward your questions to LPCXpresso forum (http://knowledgebase.nxp.com/forumdisplay.php?f=4)
0 项奖励
回复