Flashing bin to slave form master using SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing bin to slave form master using SPI

1,856 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ck1703 on Thu Jun 02 23:00:18 MST 2016
Hi,

I am using LPC54102 board as a master. I have another board which acts as a slave. I have bin file for that slave device. I want to flash that bin to slave from master (MCU) itself using SPI. How can i do that? Where should i save that slave bin file?Do i need to store that bin file in my MCU project itself? Do i need to invoke file read operations to read file? what are the possible way of falshing bin to slave?.

Thanks and Regards,
Chethan
Labels (1)
0 Kudos
Reply
2 Replies

1,761 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,761 Views
jpadilla
Community Manager

bump

0 Kudos
Reply