Hi there,
I'm trying to protect some factory configuration in my flash memory. I thought that I could protect the flash memory from being written (when this is done using the function LPC55S0XFLASH_Program or LPC55S0XFLASH_Erase).
When I configure the MPUs it seems that these functions don't trigger an exception or a hardware fault of any kind as I would expect and as it happened when I try to write in those areas by standard write operations.
Can you confirm that this is how it should happend and/or provide an alternative?
Hello, my name is Pavel, and I will be supporting your case, what kind of part are you using? is this have an S on the making number? example LPC55s69, if yes, the other alternatives that I recommend is using a signed image.
If you want to know more about this there are some apps note that could help you to setup.
The other way is modifying the CPMA and CFPA using the Flash API or using the tool Blhost through PC Host serial interface.
Best regards,
Pavel
Hello, I recommend see this links could clear more about the differences of this LPC´s.
[LPC55]: Disable ISP and SWD to utilize code protection - NXP Community
Best regards,
Pavel