Firmware dump and flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware dump and flash

2,313 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kounst on Mon Mar 14 04:28:27 MST 2016
Hi,

I somehow lost a specific built of my firmware. I have it on one device and want to copy it to run on another device.
So I'm trying to dump the FW of one device and flash it to another device.

The dump seems to be working fine using this gdb command: "dump binary memory c:/dumpfile.bin 0x0000 0xefff"
But when I flash that FW it is not working.

Any ideas why this is not working?

Thanks,
kounst
Labels (1)
0 Kudos
Reply
1 Reply

1,890 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply